|
(Read-Write) Enable/disable and query the Sample-per-Packet auto mode. Note: This command applies to FieldFox D-series (Fluyt) models and above. |
|
|
Relevant Modes |
|
|
Parameters |
|
|
<bool> |
Sample-per-packet auto mode state choose from: OFF / 0 - Disable auto mode. Enables to choose the number of samples to put in each network packet. When set to manual (and if settings is too low for the set bandwidth), FieldFox’s network speed may not keep up with the data rate. ON / 1 - Enable auto mode, packet size increases as bandwidth goes up to achieve more efficiency. |
|
Examples |
IQST:SPP:AUTO 1 'Enable auto mode. |
|
Query Syntax |
IQST:SPP:AUTO? |
|
Return Type |
bool |
|
Default |
0 |
Last Modified:
|
25May2026 |
New command for D-series models (D.14.04) and above. |