(Read-Write) Set and query the IQA data capture length via the sample number. Note: This capture length sample value is only used with a captured IQ data file. Use SENS:MEAS:CAPT:TIME to set the data capture time for the IQA data. |
|
Relevant Modes |
IQA |
Parameters |
|
<captureLength> |
Data IQA capture samples. Minimum:1 Maximum:The maximum capture length is: - 4194304 for A models and - 134217728 for B models Couplings: Capture Time. Changes will effect Capture Time (Capture Samples = Capture Time * Sample Rate + 1). |
Examples |
MEAS:CAPT:LENG 1000 |
Query Syntax |
MEAS:CAPT:TIME? |
Return Type |
integer |
Default |
12501 |
Last Modified:
05apr2019 |
Edited the default value. |
22-oct-2017 |
Added new IQA mode content (10.1x). |