(Read-Write) Set and query the filename for I/Q data capture time. Note: The Maximum value of this parameter is limited by the maximum capture samples that is available for the different platforms and determined by the current sample rate. Use SENS:MEAS:CAPT:LENGth to set the data capture time for the IQA data. Use MMEM:STOR:IQC:FTYP to set the data capture file type. |
|
Relevant Modes |
IQA |
Parameters |
|
<time> |
Data IQA capture time. Minimum:1 ps Maximum: Dynamic change. In the default setting: - Sample Rate = 12.5 MHz (A models) the max value is 335.544 ms and - Sample Rate = 125 MHz (B models), the max value is 1.07374s. |
Examples |
MEAS:CAPT:TIME 6e-6 |
Query Syntax |
MEAS:CAPT:TIME? |
Return Type |
numeric |
Default |
100 us |
Last Modified:
05apr2019 |
Corrected the min, max, and default values. |
22-oct-2017 |
Added new IQA mode content (10.1x). |