[:SENSe]:MEASurement:ADEMod (LEGACY BEHAVIOR - NOT Recommended)

(Read-Write) Set the AM/FM Metrics measurement type (Select 1 of n measurement choices)

IMPORTANT! This topic describes the Legacy Behavior for this command. This behavior is not recommended. The New behavior, which is recommended, is shown in this topic: MEAS:ADEM

Relevant Modes

SA

Parameters

NONE - Turns off the AM/FM functionality.

LAM - Tune & Listen; set demod type to AM

LFMN - Tune & Listen; set demod type to  narrow band FM

LFMW - Tune & Listen; set demod type to  wide band FM

MAM - Metrics; and set to demod type to AM

MFM - Metrics; and set to demod type to FM

<string>

 

Examples

:MEAS:ADEM NONE

Query Syntax

:MEAS:ADEM?

Return Type

String

Default

MAM


Last Modified:

01july2021

Modified topic to be a Legacy command (A.12.3x).

16-Dec-2015

Added AM/FM Metrics (8.15 & 9.15)