|
(Read-Write) Set and query the SSB auto-detection state. |
|
|
Relevant Modes |
|
|
Couplings |
When SSB auto-detect is disable, [:SENSe]:NREVm:SSB:AUTO OFF, you are able to set the various SSB settings (SSB Offset, SSB Case, Lmax and Periodicity). To use SCS auto-detection in conjunction with SSB auto-detection , set SCS to Auto. See [:SENSe]:NREVm:SCS |
|
Parameters |
|
|
<bool> |
The signal SSB auto-detection state. Choose from: OFF or 0 - Do not use SSB auto-detection for measurement. ON or 1 - Use SSB auto-detection for measurement. |
|
Examples |
NREV:SSB:AUTO ON */Sets the signal SSB auto-detection to ON |
|
Query Syntax |
NREV:SSB:AUTO? */queries the signal SSB auto-detection state |
|
Return Type |
boolean |
|
Default |
ON (1) |
Last Modified:
|
10jun2024 |
New command |