|
(Read-Write) Set and query the signal SCS. See 5G NR physical channels and modulation (3GPP TS 38.211 version 15.7.0 Release 15) Section 4.2. |
|
|
Relevant Modes |
|
|
Couplings |
AUTO parameter only available when SSB Auto-Detect is enabled. See [:SENSe]:NREVm:SSB:AUTO Other parameter only available when SSB Auto-Detect is disable. See [:SENSe]:NREVm:SSB:AUTO This setting is coupled to the Bandwidth setting. When an FR1 bandwidth is selected, 15 kHz & 30 kHz SCS are available. When an FR2 bandwidth is selected, 120 kHz & 240 kHz SCS are available. See [:SENSe]:NREVm:BANDwidth |
|
Parameters |
|
|
<char> |
The SCS value. Choose from: AUTO - Auto-detect the SCS in the measurement. S15K - 15 kHz SCS (µ = 0) S30K - 30 kHz SCS (µ = 1) S120K - 120 kHz SCS (µ = 3) S240K - 240 kHz SCS (µ = 4) |
|
Examples |
NREV:SCS AUTO */Sets the signal SCS to AUTO when SSB Auto-Detect is enabled NREV:SCS S120K */Sets the signal SCS to 120 kHz (µ=3) |
|
Query Syntax |
NREV:SCS? */queries the signal SCS value |
|
Return Type |
character |
|
Default |
AUTO |
Last Modified:
|
10jun2024 |
New command |