|
(Read-Write) Set and query the maximum number of readings the power sensor will make to achieve settling. Each power sensor reading is "settled" when either:
The readings that were taken are averaged together to become the "settled" reading. |
|
|
Relevant Modes |
FOPS (Opt 208) |
|
Parameters |
|
|
<value> |
Max number of readings. Choose a value between 1 and 20 |
|
Examples |
POIN:READ:MAX 5 |
|
Query Syntax |
[:SENSe]:POINt:READ:MAX? |
|
Return Type |
Numeric |
|
Default |
4 |
Last modified:
|
19-Mar-2014 |
New command (A.07.50) |