|
(Read-Write) Set and query the power sensor measurement tolerance. Each power sensor reading is "settled" when either:
The readings that were taken are averaged together to become the "settled" reading. |
|
|
Relevant Modes |
FOPS (Opt 208) |
|
Parameters |
|
|
<value> |
Tolerance in dB. Choose a value between 0.0 and 10.0 When consecutive power meter readings are within this value of each other, then the reading is considered settled. |
|
Examples |
TOL .05 |
|
Query Syntax |
[:SENSe]:TOL? |
|
Return Type |
Numeric |
|
Default |
.1 |
Last modified:
|
19-Mar-2014 |
New command (A.07.50) |