|
(Read-Write) Set and query the Blue power level limit used with Waterfall (SA Only) and Spectrogram displays (For SA mode, refer to Interference Analyzer 0pt 236). See also: [:SENSe]:SPECtrogram:RPLevel (Red power level) |
|
|
Relevant Modes |
SA, RTSA |
|
Parameters |
|
|
<num> |
Select the LOWEST power levels (in dB) that you expect to measure. This power level, and those measured lower than this level, appear Blue. Enter a value between the 0 and the current Red (Highest) limit. (Default Red is -50) |
|
Examples |
SPEC:BPL -80 |
|
Query Syntax |
[:SENSe]:SPECtrogram:BPLevel? |
|
Return Type |
Numeric |
|
Default |
-90 |
Last Modified:
|
19-sep-2016 |
Added RTSA as a relevant mode (A.09.50). |