[:SENSe]:SPECtrogram:RPLevel <num>

(Read-Write) Set and query the Red power level limit used with Waterfall (SA Only) and Spectrogram displays (For SA mode, refer to Interference Analyzer 0pt 236).  

See also: [:SENSe]:SPECtrogram:BPLevel (Blue power level)

Relevant Modes

SA,  RTSA

Parameters

 

<num>

Select the HIGHEST power levels (in dB) that you expect to measure. This power level, and those measured higher than this level, appear Red.

Enter a value between 0 and the current Blue (Lowest) limit. (Default Blue is -90)

Examples

SPEC:BPL -10

Query Syntax

[:SENSe]:SPECtrogram:RPLevel?

Return Type

Numeric

Default

-50


Last Modified:

19-sep-2016

Added  RTSA as a relevant mode (A.09.50).