[:SENSe]:SPECtrum:BANDwidth[:RESolution]:AUTO <bool>

(Read-Write) Set and query the Resolution Bandwidth setting. This is the resolution bandwidth of the FFT analysis. Enables or disables the FieldFox's automatic resolution bandwidth setting.

See also, If the SPEC:BAND.

Relevant Modes

IQA

Parameters

 

<boolean>

ON (1): Enables the automatic resolution bandwidth setting.

OFF (0): Disables the automatic resolution bandwidth.

Examples

SPEC:BAND:AUTO 0

SPEC:BAND:AUTO ON

Query Syntax

:SPEC:BAND:AUTO?

Return Type

numeric

Default

ON (1)


Last Modified:

22oct2017

New IQA command (A.10.1x)