(Read-Write) Set and query the FFT analysis length control. This setting is directly coupled to the resolution bandwidth as follows: Enabling Length Control (AUTO) enables the automatic resolution bandwidth setting. Disabling automatic Length Control (AUTO) to MANual, disables automatic Resolution bandwidth (i.e., Analysis length and resolution BW can be set manually). See also, If the SPEC:FFT:WIND and SPEC:FFT:ANAL:LENG. |
|
Relevant Modes |
IQA |
Parameters |
|
<boolean> |
ON (1): Enables the automatic length control setting. The FFT analysis length control is set by the FieldFox. Resolution bandwidth is set to AUTO (i.e., the automatic resolution bandwidth by the FieldFox is enabled). OFF (0): Disables the automatic length and FFT length settings. Analysis Length and resolution BW values can be set manually. |
Examples |
SPEC:FFT:LENG:AUTO 0 SPEC:FFT:LENG:AUTO ON |
Query Syntax |
:SPEC:FFT:LENG:AUTO? |
Return Type |
numeric |
Default |
ON (1) |
Last Modified:
22-Oct-2017 |
New IQA command (A.10.1x) |