[:SENSe]:SPECtrum:FFT:WINDow <char>

See also, If the SPEC:FFT:LENG:AUTO and SPEC:FFT:ANAL:LENG.

(Read-Write) Set and query the FFT filtering Window setting (spectrum analysis window ).

Relevant Modes

IQA

Parameters

 

<character>

UNIForm, TRIangular,HANNing, HAMMing, BLACkman, BH4Tap, FLAT, |FLATtop, FLAT6, FLAT7, P501, P601, KB70, KB90, KB110, GAUSsian60, GAUSsian70, GAUSsian80, SINC, TUKey25, BH3Tap, GUTop, KB80, KB100, KB120

Examples

SPEC:FFT:WIND HANN

SPEC:FFT:WIND KB70

Query Syntax

:SPEC:FFT:WIND?

Return Type

character

Default

FLATtop


Last Modified:

22-Oct-2017

New IQA command (A.10.1x)