[:SENSe]:SWEep:TYPE <char>

(Read-Write) Set and query the sweep type.

Relevant Modes

EMI, SA, RTSA

Parameters

 

<char>

Choose from:

AUTO - FieldFox chooses the sweep type that yields the most accurate data most efficiently. When ResBW is set to 200 kHz and below, FFT is selected. Above 200 kHz, STEP is selected.

FFT - Use FFT sweep.

STEP - Use STEP sweep.

Examples

SWE:TYPE STEP

Query Syntax

[:SENSe]:SWEep:TYPE?

Return Type

Character

Default

AUTO


Last Modified:

10-june-2016

Added RTSA mode (9.50)

1-Feb-2011

New command