[:SENSe]:TAListen:AM:SSB:GAIN <num>

(Read-Write) Set and query the Tune & Listen AM SSB gain value.

Unlike regular AM (AM DSB with Carrier), the optimal IF path gain cannot be automatically determined for AM SSB, so it must be configured manually. The goal is to set the gain as high as possible (to take advantage of the range of the IF and audio paths) without distorting the audio signal. It is recommended that you keep increasing the gain until you hear distortion in the audio and then back off until you no longer hear any distortion.

NOTE: The system volume setting should still be used to determine the final desired volume/level of the audio output.

See also, ADEM:METR:DYTP.

Relevant Modes

SA

Couplings

This value is only relevant when the Tune and Listen Demodulation Type is set to AM USB/LSB.

Parameters

 

<numeric>

Amount of gain (positive value) or loss (negative value) in dB.

This command will accept MIN and MAX as arguments.

Minimum: -50 dB

Maximum: 50 dB

Examples

TAL:AM:SSB:GAIN 10 'Sets the tune and listen SSB Gain to 10 dB

TAL:AM:SSB:GAIN -5 'Sets the tune and listen SSB Gain to -5 dB

Query Syntax

TAL:AM:SSB:GAIN?

Return Type

Numeric

Default

0


Last Modified:

01july2021

New command (A.12.3x)