[:SENSe]:TRIGger[:SEQuence]:PERiodic:PERiod

(Read-Write) Set and query the periodic trigger period (the time period between trigger events).

Relevant Modes

5GTF, 5G NR, 5G NR EVM Conducted, IQA,LTE FDD, PAA 

Parameters

 

<numeric>

Time in seconds.

Min: 100 us

Max: 400 ms

Examples

TRIG:PER:PER 1e-3

Query Syntax

TRIG:PER:PER?

Return Type

Numeric

Default

20 ms


Last Modified:

10dec2019

New command (11.5x)