[:SENse]:NREVm:CCARrier<n>:FREQuency:OFFSet <num>

(Read-Write) Set and query the frequency offset of the measurement from the center frequency (Measurement Frequency = Center Frequency + Offset Frequency) for the Component Carrier (CC). See also [:SENse]:NREVm:CCARrier<n>:FREQuency:CENTer

Relevant Modes

5G EVM

Parameters

 

<n>

Component carrier (CC) number. If unspecified, value is set to 1 (CC0).

n = 1 | 2 | 3 | 4 | 5

<num/char>

Frequency offset value in Hz.

MINimum (Hz): The minimum is dynamic and varies based on the Center Frequency setting and the licensed frequency range.

MAXimum (Hz): The maximum is dynamic and varies based on the Center Frequency setting and the licensed frequency range.

This command accept DEFault, MINimum and MAXimum as arguments.

Examples

NREVm:CCAR:FREQ:OFFS 2e9 */Sets the frequency offset 2 GHz for CC0

NREVm:CCAR3:FREQ:OFFS 10000 */Sets the frequency offset 10 kHz for CC2

Query Syntax

NREV:CCAR<n>:FREQ:OFFS? */queries the frequency offset of the measurement

Return Type

numeric

Default

0 Hz


Last Modified:

10jun2024

New command