SOURce:TOFFset:FREQuency <num>

(Read-Write) Set and query source tracking offset frequency.

Relevant Modes

EMI, ERTA

Parameters

 

<num>

Offset frequency in Hz.

Choose a value between 1 Hz and the maximum frequency of the FieldFox.

Examples

SOUR:TOFF:FREQ 1e3

Query Syntax

SOURce:TOFFset:FREQuency?

Return Type

Numeric

Default

0 Hz.


Last Modified:

04no2022

Added EMI mode (12.3x)

20-Jan-2015

New command (8.00)