(Read-Only) Reads the status of limit line failures. |
|
Relevant Modes |
|
Examples |
STAT:QUES:LIM:COND? The following C# excerpt assumes 4 traces, and uses a “bitwise and” of the return value: for (int i = 1; i < 5; ++i) { if ((returnValueFromScpiCommandAsInt & ((int)(Math.Pow(2, i)))) > 0) { tracePassFail[i] = "Fail"; } else { tracePassFail[i] = "Pass"; } } |
Return Type |
Numeric: 0 - All limit lines pass 2 - Any limit on trace#1 failed 4 - Any limit on trace #2 failed 8 - Any limit on trace #3 failed 16 - Any limit on trace #4 failed The returned values are added together. For example, 6 would mean traces #1 and #2 failed, 12 would mean #2 and #3 failed, 30 would mean all 4 traces failed and so forth. |
Default |
Not Applicable |
Last Modified:
04no2022 |
Added EMI mode (12.3x) |
01june2018 |
Added NF mode Opt. 356 (10.3) |
17-Jul-2012 |
Updated for A.06.00) |