SYSTem:DCPS:OUTPut <bool>

(Write-only) Enabling or disabling the output of the voltage source output.

NOTE: It is faster than turning ON/OFF DCPS voltage source output using :SYSTem:DCPS:ENABle which requires voltage ramping.

Relevant Modes

ALL Modes.

ALL models with Option 309 (Voltage Source)

Parameters

 

<bool>

Voltage source state. Choose from:

  • ON (or 1) - Enable DCPS voltage source output.

  • OFF (or 0) - Disable DCPS voltage source output.

Examples

SYST:DCPS:OUTP 1 */Enable DCPS voltage source output.

Query Syntax

N/A

Return Type

N/A

Default

N/A


Last Modified:

5Feb2026

New command for D-series (Fluyt).