SYSTem:DCPS:ENABle <bool>

(Write-only) Set the DCPS voltage source state.

To clear a 'Tripped' condition, send SYSTem:DCPS:ENABle OFF, then SYSTem:DCPS:ENABle ON or send SYSTem:DCPS:CLR.

NOTE: This command supersedes SYST:VVS:ENAB for D-series (Fluyt) models. To learn  more, refer to Replacement Commands topic.

Relevant Modes

ALL Modes.

ALL models with Option 309 (Voltage Source)

Parameters

 

<bool>

Voltage source state. Choose from:

  • ON (or 1) - Enable voltage source.

  • OFF (or 0) - Disable voltage source.

Examples

SYST:DCPS:ENAB 1 */Enable DCPS voltage source

Query Syntax

N/A

Return Type

Boolean

Default

OFF


Last Modified:

5Feb2026

New command for D-series (Fluyt).