SYSTem:PREFerences:SAADC <bool> (Superseded)

(Read-Write) Set and query the ADC Over Range Warning Emphasis.

NOTE: This command is still is supported, but has been replaced by the following command:

SYST:PREF:SA:EAOR

Relevant Modes

SA

Parameters

 

<boolean>

The Emphasis option. Choose from:

Off/False(0) - No emphasis, default warning text.

On/True(1) - Big Font and warning text and Beep sound to alert user.

Examples

SYST:PREF:SAADC 1 */Sets the ADC over range to Big Font and warning text and Beep sound to alert user.

Query Syntax

SYST:PREF:SAADC?

Return Type

boolean

Default

0


Last Modified:

01june2022

New SCPI (12.4x)