SYSTem:PREFerences:SA:EAOR:BEEP  <num>

(Read-Write) Set and query the ADC over range warning audible beep length.

NOTE: Refer to the System Settings chapter in the User's Guide for your FieldFox to learn more.

Relevant Modes

SA, RTSA

Parameters

Double

<num>

Beep length in seconds. Choose a number between 0.5 and 2 seconds.

Examples

SYST:PREF:SA:EAOR:BEEP 0.5 */Sets the audible beep to be on for 0.5s

Query Syntax

SYST:PREF:SA:EAOR:BEEP?

Return Type

Numeric

Default

0.5s


Last Modified:

21-june-23

Added to RTSA and to SA mode (A.12.7x)