SYSTem:PREFerences:STARt:MODE <char>

(Read-Write) Set and query the current Startup Mode preference.

Note: Use INST:CAT? to read the available modes on the FieldFox.

Note: Any SCPI changes to preferences require follow up "SYST:PREF:SAVE" to take effect.

See also SYST:PREF:STAR:OPT.

Relevant Modes

ALL

Parameters

 

<string>

Operating Mode. Case-sensitive. Choose from the modes that are installed on your FieldFox:

“<Default>”

Note: Depends on the FieldFox model and Options.

"CAT"

"Channel Scanner"

"CPM"

"EMI"

"ERTA"

"IQ"

"NA"

"NF"

"OTA"

"Phased Array Antenna"

"Power Meter"

"Pulse Measurements"

"RSTA"

"SA"

"VVM"

Examples

SYST:PREF:STAR:MODE "OTA" */Sets the start mode preference to "OTA".

SYST:PREF:STAR:MODE "RTSA" */Sets the start mode preference to "RTSA".

Query Syntax

SYST:PREF:STAR:MODE?

Return Type

String

Default

"<Default>"

Note: Depends on the FieldFox model and Options.


Last Modified:

01nov2022

Added new SCPI (12.6x)