(Read-Write) Set and query the current Startup Option preference that decides the FieldFox Power On behavior. Note:
Note: Any SCPI changes to preferences require follow up "SYST:PREF:SAVE" to take effect. See also SYST:PREF:STAR:MODE. |
|
Relevant Modes |
ALL |
Parameters |
|
<character> |
When set to LAST (Last Power Off State): · The last state of the FieldFox is saved on ShutDown or Restart. When the User powers on the FieldFox next time, the last state is loaded immediately. · The Startup Mode selected will be ignored during the power on sequence. · If User Preset is ON, it is set to OFF. Startup Option “Last Power Off State” takes priority.
When set to USER:
|
Examples |
SYST:PREF:STAR:OPT LAST */LAST Power Off state is enabled and the Users Preset is disabled. SYST:PREF:STAR:OPT
USER */USER preset is enabled
and the Startup mode is the first mode visible on startup |
Query Syntax |
SYST:PREF:STAR:OPT? |
Return Type |
Character |
Default |
USER |
Last Modified:
01nov2022 |
Added new SCPI (12.6x) |