|
(Write Only) Set and query the voltage source state. To clear a 'Tripped' condition, send SYSTem:VVS:ENABle OFF, then SYSTem:VVS:ENABle ON. To query the present state of the voltage source using SYSTem:VVS[:STATe]?. Note: Recommended to use SYSTem:DCPS:ENABle for D-series (Fluyt) model. |
|
|
Relevant Modes |
ALL Modes. ALL models with Option 309 (Voltage Source). |
|
Parameters |
|
|
<bool> |
Voltage source state. Choose from:
|
|
Examples |
SYST:VVS:ENAB 1 |
|
Query Syntax |
N/A |
|
Return Type |
Boolean |
|
Default |
OFF |
Last Modified:
|
5Feb2026 |
Recommended to use the "DCPS" SCPI set for D-series (Fluyt) models. |
|
20june2018 |
Updated to be Write Only |
|
23-Jul-2013 |
Added trip condition |
|
17-Jul-2012 |
New command |