|
(Read-only) Query the present Voltage Source state. Note: Recommended to use SYSTem:DCPS? for D-series (Fluyt) model. |
|
|
Relevant Modes |
ALL Modes. ALL models with Option 309 (Voltage Source). |
|
Parameters |
N/A |
|
Examples |
SYST:VVS? |
|
Return Type |
Character - Returns one of the following:
|
|
Default |
N/A |
Last Modified:
|
5Feb2026 |
Replace return type ON with INTRANSITION and READY note. Recommended to use the "DCPS" SCPI set for D-series (Fluyt) models. |
|
23-Jul-2013 |
Added tripped note |
|
17-Jul-2012 |
New command |