:TRACe:UPHase:Y:RLEVel <deg>

(Read-Write) Set and query the unwrapped phase reference level value.

See also TRAC:WAV:Y:RLEV, TRAC:REAL:Y:RLEV, TRAC:IMAG:Y:RLEV, TRAC:POL:Y:RLEV, and TRAC:PHAS:Y:RLEV.

Relevant Modes

IQA

Parameters

 

<degree>

Y-axis waveform unwrapped phase reference level.

Minimum: -360 degrees

Maximum: 360 degrees

Examples

TRAC:UPH:Y:RLEV -180

Query Syntax

TRAC:UPH:Y:RLEV?

Return Type

degrees

Default

0 degrees


Last Modified:

22oct2017

Added IQA mode (10.1x)