TRACe<n>:MEMory:UNCertainty:LOWer:DATA?

(Read-only) Read the lower uncertainty memory trace data (one value per data point -- lower uncertainty).

See also, TRAC<n>:MEM:UNC:DATA? and TRAC<n>:MEM:UNC:UPP:DATA?.

Relevant Modes

NF

Parameters

 

<n>

Trace number.

Choose from 1 to 2.

Examples

TRAC:MEM:UNC:LOW:DATA? 'Assumes n = 1
TRACe2:MEMory:UNCertainty:LOWer:DATA?

Query Syntax

See Examples

Return Type

Comma-separated numeric

Default

Not Applicable


Last Modified:

01june2018

Added NF mode Opt. 356 (10.3)