(Read-Only) Query the uncertainty lower trace data. Note: Noise Figure has asymmetric uncertainty. Noise Factor and Noise Temperature, have symmetric uncertainty. This command operates on the selected trace. First select a trace using CALC:PAR<n>:SELect. See also, TRACe<n>:UNCertainty:DATA? and TRACe<n>:UNCertainty:DATA:UPPer?. |
|
Relevant Modes |
|
Parameters |
|
| Not applicable - query only | |
Examples |
No write available |
Query Syntax |
TRACe<n>:UNCertainty:DATA:LOWer? |
Return Type |
Block data |
Default |
not applicable |
Last Modified:
01june2018 |
Added NF mode Opt. 356 (10.3) |