(Read-Only) Returns the current data X trace values. Note: In SA mode you can freeze a trace into VIEW, and then change SPAN or CF (visual effect pan/zoom). Therefore, you can get different XVAlues depending on which trace is queried (i.e., the X-value data corresponds with the trace, but not necessarily the most recent SA settings ). |
|
Relevant Modes |
EMI, ERTA, SA, RTSA |
Parameters |
|
<n> |
Trace number of data to be returned. Choose from 1 through 4. If unspecified, <n> is set to 1. |
Examples |
TRACE:XVAL? 'Assumes n = 1 TRAC2:DATA? |
Return Type |
Comma-separated numeric |
Default |
Not Applicable |
Last modified:
04no2022 |
Added EMI mode (12.3x) |
01june2019 |
New command (11.26) |