|
(Read-Write) Set the trigger frame offset. This command lets you advance the phase of the frame trigger by the amount you specify. It does not change the period of the trigger waveform. If the command is sent multiple times, it advances the phase of the frame trigger an additional amount each time it is sent. See also period frame offset reset. |
|
|
Relevant Modes |
RTSA |
|
Parameters |
|
|
<num> |
Range: 0 to 100 ms |
|
Examples |
TRIG:FRAM:OFFS 1.6 ms |
|
Query Syntax |
[:SENSe]:FRAM:OFFS? |
|
Return Type |
numeric |
|
Default |
0.00000000 |
Last Modified:
|
19-sep-2016 |
Added new RTSA command (A.09.50). |