|
(Write-Only) Resets the trigger frame offset to 0. Resets the value of the periodic trigger frame offset display setting to 0.0 seconds. The current displayed trigger location may include an offset value defined with the Offset key. Pressing this key redefines the currently displayed trigger location as the new trigger point that is 0.0 s offset. The Frame Offset SCPI can then be used to add offset relative to this new timing. |
|
|
Relevant Modes |
RTSA |
|
Parameters |
|
|
<Bool> |
|
|
Examples |
TRIG:FRAM:OFFS:DISP:RES |
|
Query Syntax |
n/a |
|
Return Type |
n/a |
|
Default |
0.00000000 |
Last Modified:
|
19-sep-2016 |
Added new RTSA command (A.09.50). |