|
(Read-Write) Set and query the trigger position. Available ONLY in Zerospan measurements. This is an easy way to automatically set the Trigger Delay by positioning the trigger event (also known as T zero) at any graticule along the X-axis. Also set TRIGger[:SEQuence]:POSition:STATe |
|
|
Relevant Modes |
SA |
|
Parameters |
|
|
<num> |
Trigger position. Choose a value from 0 to 10: 0 - T zero occurs at the left graticule. 5 - T zero occurs at the center of the screen. 10 - T zero occurs at the far right graticule. |
|
Examples |
TRIG:POS 5 |
|
Query Syntax |
TRIGger[:SEQuence]:POSition? |
|
Return Type |
Numeric |
|
Default |
0 |
Last Modified:
|
28-Mar-2013 |
New command (6.25) |