:TRIGger[:SEQuence]:POSition:STATe <bool>

(Read-Write) Set and query the trigger position state. Set trigger position using TRIGger[:SEQuence]:POSition.

Relevant Modes

SA

Parameters

 

<bool>

Trigger position state. Choose from:

OFF or 0 - Trigger position OFF.

ON or 1 - Trigger position ON. TRIGger[:SEQuence]:DELay is set automatically and can NOT be overwritten.

Examples

TRIG:POS:STAT 1

Query Syntax

TRIGger[:SEQuence]:POSition:STATe?

Return Type

Boolean

Default

OFF (0)


Last Modified:

22-044-2026

New command