|
(Read-Write) Set and query the source of trigger signals which initiate a measurement. See Trigger:Source command for NA Mode. |
|
|
Relevant Modes |
|
|
Parameters |
|
|
<char> |
Choose from: FREerun - The USB Power Sensor acquires data without waiting for a trigger. This mode is NOT supported for Trace Graph measurements. INTernal - The USB Power Sensor acquires data when a valid pulse signal is detected at the RF input. The following Trigger settings determine the validity of the trigger signal. EXTernal - The USB Power Sensor acquires data when a valid TTL signal is detected at the USB Power Sensor external trigger input. |
|
Examples |
TRIG:SOU EXT |
|
Query Syntax |
TRIGger:SOUrce? |
|
Return Type |
Character |
|
Default |
INTernal |
Last Modified:
|
30-May-2014 |
New command |