|
(Read-Write) Set and query the source of trigger signals which initiate a measurement. See Trigger:Source command for Pulsed Measurements Mode. |
|
|
Relevant Modes |
|
|
Parameters |
|
|
<char> |
Choose from: INTernal - Sweeps are initiated by the FieldFox internal circuitry. EXTernal - A sweep is initiated on the rising or falling edge of an external TTL signal at the Ref In/Trig In connector on the FieldFox top panel. POINt - An exteral trigger type that acquires exactly one data point per trigger input. |
|
Examples |
TRIG:SOUR EXT |
|
Query Syntax |
TRIGger:SOURce? |
|
Return Type |
Character |
|
Default |
INTernal |
Last Modified:
|
06mar2025 |
Added a new POINt parameter to the command. |
|
6-Mar-2013 |
New command (6.25) |