Source and Analyzer (single-point only)

When you select Source and Analyzer (single-point only) in the Calibration Wizard Setup dialog, the Calibration Wizard is configured to calibrate a single point for both the source and analyzer hardware in the following steps:

  1. Connect for Analyzer Calibration
  2. Analyzer Calibration Measurement
  3. Connect for Source Calibration
  4. Source Calibration Measurement
  5. Calibration Complete

For source and analyzer multi-point calibration, you need to perform a separate calibration for each (e.g., run the Calibration Wizard for multi-point analyzer to generate a set of corrections files for the analyzer hardware, then do the same for the source hardware.