Download All Signals Auto Range Acquisition Input Acquisition Disconnected Calibration Wizard Acquisition Connected

System Tools

This topic describes the System Tools area. Click a region on the image to go to a description.

The System Tools manage the signal processing with the source and analyzer hardware.

Download All Signals

Downloads all signals in the Signals resource panel to the selected source hardware, making them available for acquisition.

Auto Range Acquisition Input

Auto Range Acquisition Input automatically sets the optimum full scale amplitude range for the input signal. You can use the Auto Range Acquisition Input button on the Signal Optimizer to quickly start an autorange. It samples the current input signal and then sets the full scale input range to the minimum range that includes the peak voltage sample of the input signal.

When the Signal Optimizer performs auto range, two changes are made to the measurement setup before measuring (sampling) the input signal:

Auto Range Acquisition Input may make more than one measurement to complete the process. If the first measurement detects an overload condition, the input range is increased and another measurement made. If the new autorange setting changes more than 15 dB then another measurement made to verify the new setting is correct.

General Auto Range Procedure

In general, Auto Range is an estimate of an input range setting that will work, but will not provide optimal results. The specifics for finding the optimal input range setting vary depending on the hardware configuration type and measurement type, but in general follows the procedure below:

  1. Configure desired signal to be present at input to the analyzer
  2. Confirm the signal is present at the expected frequency/power with the Time & Spectrum measurement.
  3. Configure the basic measurement settings (center frequency, span, measurement properties, etc.).
  4. Perform an Auto Range operation and make some measurements.
  5. Observe the measurement results desired for optimization (probably something like an EVM metric).
  6. If an overload indicator is present, increase the input range or input range offset property of the analyzer until the indicator disappears.
  7. As the input range or input range offset property of the analyzer is stepped up and down, observe the measurement result and choose the setting which optimizes the result. Note in some cases an overload indicator may be present when this is optimized, and indicates the noise level and distortion trade-offs for that configuration are best served by allowing a small amount of signal clipping.

Auto Range Limitations

Auto Range Acquisition Input works well for most common input signals. Signals that don't work as well are:

Some models of the oscilloscopes (those with very high maximum sample rates) are vulnerable to the measurement span issue mentioned above. Also, the Zoom property in oscilloscopes can include image related energy in the measurement that will cause auto-range to end up on a range too high.

For the Z9070B hardware configuration, the auto-range function does not work and results in an input range setting that may be off by as much as 20 dB. It is recommended to use a manual approach for choosing input range setting when using a Z9070B hardware configuration.

Acquisition Disconnected

The input signal to the analyzer hardware is currently disconnected. Click this button to connect it.

Acquisition Connected

The input signal to the analyzer hardware is currently connected. Click this button to disconnect it.

Calibration Wizard

Opens the Calibration Wizard Setup window where you can begin configuring both single-point and multi-point system calibrations. Refer to the Calibration Wizard topic to learn more.