Configure PC to Analyzer over GPIB

This procedure shows how to connect the PC to analyzer using a GPIB cable.

Important Note

This connection method can NOT be used for the following PNA models/firmware versions:

  • All PNA C models with firmware versions below A.09.42.18

  • All PNA/PNA-X models with firmware versions below A.09.50.12

  • All other older PNA models.

Use Configure PC to Analyzer over LAN method with the additional Step 4.

Procedure

  1. Connect GPIB interface cable between the PC and the analyzer.

  2. Run N1500A Software. Click Preferences, then Select Instrument, then Re-Scan. The software will automatically try to connect to the GPIB instrument.

  3. If the connection dialog does NOT show the GPIB instrument, use Keysight IO Libraries to verify that the instrument was properly configured.