The following images demonstrate the changes that occur when pre-emphasis and de-emphasis is used in a Multi-channel eye diagram.
Note the Y-axis scaling differences.
To see the bit pattern waveform, click the right icon on the Parameter Format Selection pane. Learn how.

The lower amplitude is 200 mV and the higher amplitude is 400 mV

The lower amplitude is 100 mV and the higher amplitude is 200 mV