This feature allows you to open or import multiple files simultaneously. Files are opened into the same initial view.

|
Important!
|
Select Data Domain -
|
Important!
|
Select Files to Open or Import. Click Add, then click Files of type and select the file type to open or import.
DUT Configuration - All DUT files must share the same DUT configuration (4-port, 8-port and so forth). Click Change to launch the DUT configuration dialog.
Limit Data Range to Open / Import
All - All files retain their original data range.
Subset - The stimulus range for all files will assume the specified Start, Stop, Points and Step settings. The frequency range must be the same, or a subset of the original two files. It can NOT be larger than the data provided by the original two files.
Interpolate May be checked automatically by PLTS if a subset setting is made that requires Interpolation. Interpolated data is not as accurate as measured data.
Checked - Subset settings have been changed that require the imported data to be interpolated.
Cleared - Imported data is NOT interpolated.
Reset Returns the Subset settings to the original values.
Click OK to Open or Import Data