DUT Configuration


To see this dialog, at the PLTS Wizard Welcome dialog, click Edit. This dialog can also be accessed by selecting File -> Import -> Single File then clicking on the Change button in the Import a Single File dialog.

DUT Configuration dialog

These selections are best made in the specified order.

When each step is selected, the appropriate field in the diagram below becomes available and remains available while subsequent steps are selected.

1. Enter the number of DUT ports to calibrate and measure. Beginning with PLTS 2018, the maximum number of DUT ports is 64.

Or click Load to recall a previously saved configuration (*.dcf) file.

Quick Topologies for 2, 3, or 4 Ports

For convenience, when 2, 3, or 4 ports are selected, then select from the following topologies:

2-ports

Single Ended - Single Ended

Differential Reflection

3-ports

Differential - Single Ended

Single Ended - Single Ended

4-ports

Differential - Differential

Differential - Single Ended

Single Ended - Differential

Single Ended - Single Ended

Quick Topologies

This quick topology interface allows you to choose a DUT-port assignment for 2, 3, 4, 6, or 8 ports. Although each graphical configurations shows 8 ports, it assigns only the number of ports you selected to measure. The example images below show the options available for a 3-port configuration.

 

2. Change DUT Configuration  On the diagram below, click...

Indicates Differential port

Indicates Single-ended port

Uncouple Adjacent Differential Ports on a Differential Thru (this is a convenience setting).

  • When cleared (default setting), clicking the DUT configuration symbol (Differential or Single-ended) on either the Input or Output will change the other automatically.

  • When checked, the Input and Output is changed independently.

3. Change Logical port numbers.  For differential pairs, the logical port is comprised of two DUT ports. For single-ended ports, the logical port can be a different number than the DUT port.

4. Change the DUT port numbers (DUT Port).

Logical ports are comprised of the adjacent single-ended DUT ports.

5. Specify a more descriptive label. For the PNA/ Single-ended DUT port. The text replaces input and output arrows (<<<< and  >>>>).

6. Change the VNA port used to measure the DUT. The E5071C ENA has some limitations that must be considered. See E5071C Limitations.

DUT Configuration

Description  File name of the current configuration. Change this text, then click Save As to store the current configuration to a *.dcf file using this file name.

Save As  Store the current configuration. This file can later be recalled using the Load button.

OK  Applies current settings to the measurement and closes the dialog.

Cancel  Discards the changes you made since open the dialog and closes the dialog.

Reset  Recall the Default Configuration.