Click an object to access its properties and methods.
The PLTS API supports:
C++
C#
VEE
Visual Basic
More programming examples are provided with the PLTS Installation at:
C:/Program Files/Keysight/PLTS_xx/APISamples
Where xx is the latest PLTS release.
When controlling PLTS remotely, you may have to disable the UAC. This will occur when the remote computer Operating system is Windows Vista, Windows 7 and Windows Server 2008 operating system. Learn how.