Write/Read |
About Exporting Data |
Description |
Sets and reads the data range to export. To export data, use ExportFreqDomainTextFileWithSpecifiedDefaults Method or ExportTimeDomainTextFileWithSpecifiedDefaults Method. |
VB Syntax |
doc.ExportDataRange = range |
Variable |
(Type) - Description |
|
doc |
(object) - A PLTSDoc object |
|
range |
(Enum as pltsDataRange) Range to export. Choose from: 0 - RangeAll - Export the entire data range in PLTS memory. 1 - Subset The data range is specified with the start freq/time, stop freq/time and step freq/time properties. |
Return Type |
Enum |
Default |
RangeAll (0) |
Examples |
doc.ExportDataRange = Subset |
C++ Syntax |
HRESULT get_ExportDataRange(tag pltsDataRange* Value); HRESULT put_ExportDataRange(tag pltsDataRange Value); |
Interface |
IPLTSDoc |