Write/Read | 
About Exporting Data | 
Description | 
 Sets and reads the CHANGED port mapping for exported text files. (Use this command ONLY if you change the DUT port mapping in an exported text file.) 
 To export data, use ExportFreqDomainTextFileWithSpecifiedDefaults Method or ExportTimeDomainTextFileWithSpecifiedDefaults Method.  | 
|
VB Syntax | 
 doc.ExportDiffPortMap = portMap  | 
|
Variable | 
(Type) - Description | 
|
| 
 doc  | 
 (object) - A PLTSDoc object  | 
|
| 
 portMap  | 
 (String) Port map after export. See example below.  | 
|
Return Type | 
 String  | 
|
Default | 
 " " (empty string) - Do NOT change port mapping.  | 
|
Example | 
 Manually Export data with the following GUI port mapping: 
 Open the exported text file and copy the header information: 
 Command string: doc.ExportDiffPortMap = "1|2P|2|2P|0|UC|0|UC|" doc.ExportPortMap = "2|1|<<<<<<|1|2|>>>>>>|3|3|<<<<<<|4|4|>>>>>>|"  | 
|
C++ Syntax | 
 HRESULT get_ExportDiffPortMap(BSTR *Value); HRESULT put_ExportDiffPortMap(BSTR Value);  | 
|
Interface | 
 IPLTSDoc  |