Write/Read |
About Exporting Data |
Description |
Sets and reads whether to export gated frequency domain data. Gated data is ONLY available when:
To export data, use ExportFreqDomainTextFileWithSpecifiedDefaults Method. |
VB Syntax |
doc.ExportGatedData = value |
Variable |
(Type) - Description |
|
doc |
(object) - A PLTSDoc object |
|
value |
(Boolean) 0- False Ungated, calibrated data is exported. 1 - True Gated data is exported. |
Return Type |
Boolean |
Default |
0 - False |
Examples |
doc.ExportGatedData = False |
C++ Syntax |
HRESULT get_ExportGatedData(Variant_Bool *Value); HRESULT put_ExportGatedData(Variant_Bool Value); |
Interface |
IPLTSDoc |