Write/Read |
About Exporting Data |
Description |
Sets and reads whether to export all data in one file or to separate files. To export data, use ExportFreqDomainTextFileWithSpecifiedDefaults Method or ExportTimeDomainTextFileWithSpecifiedDefaults Method. |
VB Syntax |
doc.ExportInOneFile = value |
Variable |
(Type) - Description |
|
doc |
(object) - A PLTSDoc object |
|
value |
(Boolean) 0 - False All selected parameters are saved to separate files. Each file is saved to the specified folder with the filename you entered and a parameter label appended to the name. For example, if you entered device4 as the file name, the S11 parameter file is named: device4_S11.txt. 1 - True All selected parameters are saved to one file. |
Return Type |
Boolean |
Default |
1 - True |
Examples |
doc.ExportInOneFile = False |
C++ Syntax |
HRESULT get_ExportInOneFile(Variant_Bool *Value); HRESULT put_ExportInOneFile(Variant_Bool Value); |
Interface |
IPLTSDoc |