Write/Read | 
About Exporting Data | 
Description | 
 Sets and reads a comma-delimted list of parameters to export. A list is ONLY used when TextFileDataToExport is set to "Customized". To export data, use ExportFreqDomainTextFileWithSpecifiedDefaults Method or ExportTimeDomainTextFileWithSpecifiedDefaults Method.  | 
VB Syntax | 
 doc.ExportParamList = value  | 
Variable | 
(Type) - Description | 
| 
 doc  | 
 (object) - A PLTSDoc object  | 
| 
 value  | 
 (String) List of parameter to export separated by commas.  | 
Return Type | 
 String  | 
Default | 
 Not Applicable  | 
Examples | 
 doc.ExportParamList = "S11,S12,SDD11" ' Frequency domain parameters doc.ExportParamList = "T11,T12,TDD11" ' Time domain parameters  | 
C++ Syntax | 
 HRESULT get_ExportParamList(BSTR *Value); HRESULT put_ExportParamList(BSTR Value);  | 
Interface | 
 IPLTSDoc  |