Write-only |
About Views |
Description |
Saves a picture of the view. Use DrawPlot to plot data in the view before calling this command. This function exports what you see in the view. If the view is blank, a blank picture is exported. |
VB Syntax |
pltsView.ExportPlots (FilePath, pictureWidth, pictureHeight) |
Variable |
(Type) - Description |
|
pltsDoc |
(object) - A PLTSView object |
|
FilePath |
(String) Full path and file name of the picture. The file extension is used to determine picture format. Supported file extensions are “.bmp”, “.png”, “.jpg” and “.gif”. The directory must exist. |
|
pictureWidth |
(short) Picture width in pixels. |
|
pictureHeight |
(short) Picture height in pixels. |
Return Type |
Not Applicable |
Default |
None |
Examples |
pltsView.ExportPlots "C:\Users\guest\temp\MyView.png, 400,200 |
C++ Syntax |
HRESULT ExportPlots(BSTR outputPictureFilePath, SHORT pictureWidth, SHORT pictureHeight); |
Interface |
IPLTSView |